DDR Validation Tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DDR Validation Tool

2,332件の閲覧回数
justinjonas
Contributor III

When I run the DDR validation tool, I don't see any scenarios for the 'Validation Stage'. I want to use these scenarios to properly configure the DDR3L chip I am using. I am using CodeWarrior for ARMv8 targeted at the LS1012A processor. Is there anything I need to do to get these scenarios to appear?

ddrvalidation.PNG

Thanks for your help.

タグ(1)
0 件の賞賛
返信
3 返答(返信)

2,093件の閲覧回数
addiyi
NXP Employee
NXP Employee

DDR controller from LS1012 board doesn't provide wrlv clock adjust and there are no registers for that. We don't have  in this moment an algorithm for DDR tuning for this SoC.

Adrian 

0 件の賞賛
返信

2,093件の閲覧回数
justinjonas
Contributor III

Do you have any suggestions as to debug or tune a DDR chip with the LS1012?

0 件の賞賛
返信

2,093件の閲覧回数
addiyi
NXP Employee
NXP Employee

The DDR controller for LS1012 is very simple, so a working DDR configuration is enough for having a good configuration. Controller doesn't provide a way for fine tuning, it will just work or not.

Adrian

0 件の賞賛
返信