Continuous self test / Built In Test for T1042 SoC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Continuous self test / Built In Test for T1042 SoC

1,380件の閲覧回数
antoinedurand
Contributor II

Does a Continuous Self Test, Built In Test, monitoring mecanism exist for T1042, which could be run on top of linux Operating System ?

Thanks.

0 件の賞賛
返信
1 返信

1,214件の閲覧回数
Pavel
NXP Employee
NXP Employee

The T1042 DDR controller has means for automatic memory testing.

Please refer to the QorIQ T1042 Reference Manual, 14.4.59 DDR Memory Test Control Register (DDR_DDR_MTCR) and next sections.

 

See also the Section 1.3.3.1 of the "QCVS SerDes Tool User Guide":

https://www.nxp.com/docs/en/user-guide/QCVS_SerDes_User_Guide.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信