Continuous self test / Built In Test for T1042 SoC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Continuous self test / Built In Test for T1042 SoC

1,362 次查看
antoinedurand
Contributor II

Does a Continuous Self Test, Built In Test, monitoring mecanism exist for T1042, which could be run on top of linux Operating System ?

Thanks.

0 项奖励
回复
1 回复

1,196 次查看
Pavel
NXP Employee
NXP Employee

The T1042 DDR controller has means for automatic memory testing.

Please refer to the QorIQ T1042 Reference Manual, 14.4.59 DDR Memory Test Control Register (DDR_DDR_MTCR) and next sections.

 

See also the Section 1.3.3.1 of the "QCVS SerDes Tool User Guide":

https://www.nxp.com/docs/en/user-guide/QCVS_SerDes_User_Guide.pdf


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复