CPU1 failed to come online

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CPU1 failed to come online

3,914 Views
alessandromarin
Contributor I

Hello, can anyone help me please?

 

I am trying to enable the second cpu of a dual core ARMv7 ls1021a Processor.

The kernel version used is 4.1.8-rt8+ls1.

 

Douring start up operations I obtain the following message:

 

CPU1: failed to come online

 

Thank you

0 Kudos
Reply
3 Replies

3,012 Views
ufedor
NXP Employee
NXP Employee

Which board is in question?

If it is a proprietary one - please provide the schematics as searchable PDF.

If the schematics can be provided only confidentially please create a Technical Case:

How I could create a Service Request? | NXP Community 

Which NXP SDK is used?

Please provide complete U-Boot log as text file.

0 Kudos
Reply

3,008 Views
alessandromarin
Contributor I

Thanks for your kind help,

The board in question is an LS1021ATWR.

The NXP SDK used is: QorIQ-SDK-v2.0-20160527-yocto

I have saved all the messages coming out from u-boot and from the linux boot loader in the attached file.

Please tell me if you need more information.

0 Kudos
Reply

3,008 Views
ufedor
NXP Employee
NXP Employee

Please try to use pre-compiled images from the QorIQ Linux SDK v2.0 CORTEXA7 IMAGE.iso

0 Kudos
Reply