CAN KE06 Filter MASK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN KE06 Filter MASK

1,337 Views
christianquanti
Contributor I

I am configuring the CAN.
I added a filter only for ID 0x7EB.
The value of CANIDMR0 / 1 and CANIDAR0 / 1 with 0xFD600000, but other ID's are working.
I am using KDS3.2 and MKE06Z128VLH4.
Can you help me?

Tags (1)
0 Kudos
Reply
1 Reply

1,278 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Christian Vieira ,

  If you just want to receive one ID, then you can configure CANIDMR to 0, check each bit, just when the received ID is totally the same as the IDAR, it will be received.

If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply