Boot Type

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Boot Type

1,397 Views
Zhoute
Contributor I

Is there a relationship between the connection of LX2080 to the CodeWarrior emulator and the boot mode? Currently, my RCW_SRC[3:0] is configured as “1111”,Boot via NOR Flash

0 Kudos
Reply
1 Reply

1,379 Views
June_Lu
NXP TechSupport
NXP TechSupport

If there is available firmware in the NOR, you could use this configuration.

If there is no firmware, and it's the first time you connect the LX2080, it's bareboard, please set the RCW_SRC[3:0] to hard-code.

When you connect the CodeWarrior TAP, should confirm the board could complete the Power-On Reset Sequence.

LX2160A Reference Manual,

4.9.5 Power-On Reset Sequence Detailed Description, step 24, System Ready State.

4.9.6 Power-On Reset Sequence Timing

Thanks

0 Kudos
Reply