Time Sensitive Networking on LS1028ARDB

cancel
Showing results for 
Search instead for 
Did you mean: 

Time Sensitive Networking on LS1028ARDB

Time Sensitive Networking on LS1028ARDB

Time Sensitive Networking(TSN) is an extension to traditional Ethernet networks, providing a set of standards compatible with IEEE 802.1 and 802.3. TSN aims to provide guarantees for deterministic latency and packet loss under congestion, allowing critical and non-critical traffic to be converged in the same network. This document introduces basic concept of Time Sensitive Networking, LS1028 TSN switch and using TSN features on LS1028ARDB.

TSN Introduction

TSN in LS1028

Using TSN features on LS1028ARDB

Attachments
Comments

Time Sensitive Networking(TSN) is an extension to traditional Ethernet networks, providing a set of standards compatible with IEEE 802.1 and 802.3. TSN aims to provide guarantees for deterministic upsers portal latency and packet loss under congestion, allowing critical and non-critical traffic to be converged in the same network.

Version history
Revision #:
1 of 1
Last update:
‎09-14-2019 03:30 AM
Updated by: