!!!!! ltib glibc build failed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

!!!!! ltib glibc build failed

3,792件の閲覧回数
zhengwang
Contributor I

hello everyone:

did someone meet the following problem?

the glibc version i have used:

glibc-headers-2.5-81.el5_8.7

glibc-common-2.5-81.el5_8.7

glibc-devel-2.5-81.el5_8.7

glibc-utils-2.5-81.el5_8.7

glibc-2.5-81.el5_8.7

meet the conditions for installing ltib >2.2.x


when i input the command "./ltib -c", the question occurs:


[/home/xxx/ltib-p2020rdb-20100428/rpm/BUILD/glibc-2.10.1/build-glibc/socket/sa_len.o] Error 1

make[2]: *** Waiting for unfinished jobs....

make[2]: Leaving directory `/home/xxx/ltib-p2020rdb-20100428/rpm/BUILD/glibc-2.10.1/socket'

make[1]: *** [socket/subdir_lib] Error 2

make[1]: Leaving directory `/home/xxx/ltib-p2020rdb-20100428/rpm/BUILD/glibc-2.10.1'

make: *** [all] Error 2

error: Bad exit status from /home/xxx/ltib-p2020rdb-20100428/tmp/rpm-tmp.86727 (%build)

RPM build errors:

    Bad exit status from /home/xxx/ltib-p2020rdb-20100428/tmp/rpm-tmp.86727 (%build)

Build time for glibc-2.10: 261 seconds

Failed building glibc-2.10

f_buildrpms() returned an error, exiting

traceback:

main:560

Started: Tue Oct  9 14:16:40 2012

Ended:   Tue Oct  9 14:22:14 2012

Elapsed: 334 seconds

These packages failed to build:

glibc-2.10

Build Failed

in the dir "/home/xxx/ltib-p2020rdb-20100428/rpm/BUILD/glibc-2.10.1/build-glibc/socket/"

i cannot find the files of sa_len.o and subdir_lib, and sa_len.o.dt is a empty file。the normal files are coexisting with the "****.o " and "****.o.dt" formats.

help me please! i'm new in embeded linux developing

thank u very much.

[email protected]


ラベル(1)
0 件の賞賛
返信
2 返答(返信)

3,043件の閲覧回数
zhengwang
Contributor I

isn't the key of the problem that the version of glibc for my linux os centos 5 is 2.5.81, but the glibc version of my ltib is 2.10?

if so ,how can solve it ?

0 件の賞賛
返信

3,043件の閲覧回数
zhengwang
Contributor I

it's amazing!!!!

why i change the configuring parameter of glibc to uclibc, build failed, and prompt the message "kernel-2.6.x build failed"

and then i change back to be glibc, build successed!!!

what's wrong???

0 件の賞賛
返信