The differences between alternate functions and muliplex options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The differences between alternate functions and muliplex options

1,945 Views
xiangwei
Fresh Out Contributor

Hi,everyone!

    In P1021RM,table3-10 (page 127) has listed the QUICC Engine Multiplex pins.For example, CE_PA0 has alternative functon of LAD8,but in table 3-7(page 119),CPPARAx[SELn] has no option for LAD8.

    1. That mean that,i can use LAD8 and QUICC sub-function  simultaneously ?for e.g.

      for CE_PA0 ,  I set CPPARAx[SELn] to 11,then PA0 used for UPC1_S_TxADDR[4]. Following a utopia interface opration,the CPU can initial a eLBC access through LAD8 without any change of CPPARAx[SELn] value?

      2.What's the defferences of 'alternate function' and 'muliplex option'?

      Thanks!

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,764 Views
LPP
NXP Employee
NXP Employee

P1021 QE pins are muxed with non-QE signals. The selection between QE and non-QE function is performed via PMUXCR bits.

Please, read description of QE1 field in RM Section 20.5.7

>What's the defferences of 'alternate function' and 'muliplex option'

PMUXCR selects between QE and non-QE alternate functions.

CPPARAx provides further selection between QE options.

Do not not attach particular importance to the terms. They are interchangeable.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply