Is it possible to run more than one USDPAA application at once?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to run more than one USDPAA application at once?

ソリューションへジャンプ
1,708件の閲覧回数
jorhai
Contributor II

I notice that the USDPAA "dma_mem" driver prevents more than one USDPAA application running in the same time.

But we have to add USDPAA to multi-process. Is it possible?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,446件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello sf dong,

It is possible to run multiple USDPAA applications at the same time, please make sure they use different buffer pools.

You need to modify the dts file to make different applications to use different Ethernet ports which use different buffer pools.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,447件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello sf dong,

It is possible to run multiple USDPAA applications at the same time, please make sure they use different buffer pools.

You need to modify the dts file to make different applications to use different Ethernet ports which use different buffer pools.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信
1,446件の閲覧回数
jorhai
Contributor II

Hi Yiping.

          Thanks for your kindly reply.

          I will try it.

          But it is using the same DMA_mem while  seeding different buffer pools in multiple USDPAA applications. Will it cause overlay to memory.

          Thanks again.

           dongsf.

0 件の賞賛
返信