Is it possible to run more than one USDPAA application at once?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Is it possible to run more than one USDPAA application at once?

Jump to solution
1,703 Views
jorhai
Contributor II

I notice that the USDPAA "dma_mem" driver prevents more than one USDPAA application running in the same time.

But we have to add USDPAA to multi-process. Is it possible?

Labels (1)
0 Kudos
Reply
1 Solution
1,441 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello sf dong,

It is possible to run multiple USDPAA applications at the same time, please make sure they use different buffer pools.

You need to modify the dts file to make different applications to use different Ethernet ports which use different buffer pools.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
1,442 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello sf dong,

It is possible to run multiple USDPAA applications at the same time, please make sure they use different buffer pools.

You need to modify the dts file to make different applications to use different Ethernet ports which use different buffer pools.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply
1,441 Views
jorhai
Contributor II

Hi Yiping.

          Thanks for your kindly reply.

          I will try it.

          But it is using the same DMA_mem while  seeding different buffer pools in multiple USDPAA applications. Will it cause overlay to memory.

          Thanks again.

           dongsf.

0 Kudos
Reply