u-boot does not boot from emmc

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

u-boot does not boot from emmc

3,639 Views
niharunadkat
Fresh Out Contributor

Hi,

I am trying to boot from an emmc and this is the error message i get when my ARM units boots

U-Boot SPL 2017.11 (Jul 31 2019 - 11:45:24)                                     
Initializing DDR....using SPD                                                   
Trying to boot from MMC1                                                        
mmc_init: -110, time 43                                                         
spl: mmc init failed with error: -110                                           
SPL: failed to boot from all boot devices                                       
### ERROR ### Please RESET the board ###

I can use the same u-boot-with-spl-pbl.bin and boot from and SD card. What i am missing?

Please provide any information for the issue seen# above.

Thank you

Nihar

0 Kudos
Reply
1 Reply

3,443 Views
ZhangJennie
NXP TechSupport
NXP TechSupport
0 Kudos
Reply