synchronizing processor expert project with service

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

synchronizing processor expert project with service

2,212件の閲覧回数
nikolayyakovenk
Contributor III

When exported and imported the Project, and IDE tries to open processor expert, the IDE hangs displaying "synchronizing processor expert project with service". If to leave like that after 20 minutes or so Java gets stack overflow. To continue use the project I have to kill or rename ProcessorExpert.pe so the project can be used with already generated PE code. I was never been able to restore PE operation with this project anymore.

0 件の賞賛
返信
3 返答(返信)

2,045件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Nikolay ,

Which chip do you used ?

The problme only occur on this proejct  ? What about any other projects ?

BR

Alice

0 件の賞賛
返信

2,045件の閲覧回数
nikolayyakovenk
Contributor III

Yes Alice,

Thanks for your interest in helping.

This is a single occurrence. In the beginning it was happening during exporting/importing , but original project was working for some time but then started to hang as well. The project is rather big -- there are 12 drivers configured.

I did try a simpler projects and export/import went fine.

I can continue modifying drivers manually without using PE, since PE always hangs like that. I kinda lost hope to fix it so I just renamed ProcessorExpert.pe to some other extension so it will not try to “synchronize with the service” anymore. ☺

The micro is S32K144_64.

Regards,

Nik.

0 件の賞賛
返信

2,045件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Nik,

Thanks for your sharing.

BR

Alice

0 件の賞賛
返信