sbc_fs651 component is not available in processor expert of mpc5777c controller.

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

sbc_fs651 component is not available in processor expert of mpc5777c controller.

2,354 次查看
Krishnayya29
Contributor I

Hi Nxp,

 

when i import SBC example from NXP for MPC5777c controller, IDE Says that  sbc_fs651 is not installed in this version .Could you please help me out to enable this component to make this example work properly. i am using ide  S32DS power 2.1  and RTM 3.0.3 SDK version.i pasted image that shows  error messages and disabled component below.

Krishnayya29_0-1681910361547.png

Please let me know if i need to communicate with SBC via SPI component, if  sbc_fs651 is not available for this controller or SDK.

Thanks,

Krishnayya

0 项奖励
回复
4 回复数

2,261 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Have a look at this thread where one customer solved this issue:

https://community.nxp.com/t5/MPC5xxx/I-get-the-following-error-when-i-laund-the-S32-IDE/m-p/1616682#...

Best regards,

Peter

0 项奖励
回复

2,338 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hmm, I have just opened new project from example and everything looks fine.

petervlna_0-1681976945720.png

Do you have the correct components installed?

petervlna_1-1681977030028.pngpetervlna_2-1681977088097.png

Best regards,

Peter

0 项奖励
回复

2,335 次查看
Krishnayya29
Contributor I

Hi Peter,

Thanks for the quick reply.i am not getting option to select version PA15 or PA11 as you.i need to install PA15  SDK version.can you please guide me to  to install PA15sdk .

the pop up i am getting from IDE is pasted below.

Krishnayya29_0-1681979159523.png

Thanks,

Krishnayya

 

0 项奖励
回复

2,289 次查看
Krishnayya29
Contributor I

Hi Peter,

 

Could you please tell me what i am doing wrong while installing or which version i need to install to work with SBC.presently i am using S32DS power architecture 2.1 version and SDK 3.0.3.

 

Thanks,

Krishnayya

0 项奖励
回复