kernel boot set display resolution

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

kernel boot set display resolution

3,625 Views
Egor_I_InertgasM
Contributor II

I have Variscite Symphony board on imx8mp SoM with LVDS panel and HDMI output.

I replaced psplash image. Image on the LVDS panel fits into panel resolution 800x480. And I do not use LVDS panel, I leave default settings from the vendor.

But the image on the HDMI panel 800x600 places into the top left corner.

I set HDMI resolution later in weston.ini.

But how can I set HDMI resolution at kernel boot or fit psplash image into HDMI display?

0 Kudos
Reply
2 Replies

3,544 Views
Egor_I_InertgasM
Contributor II

disabling LVDS panel in the device tree makes splashscreen on the HDMI panel better

0 Kudos
Reply

3,600 Views
igorpadykov
NXP Employee
NXP Employee

Hi Egor

 

i.MX8M Plus HDMI supports only CEA modes (800x600 is not CEA resolution) as described in

sect.13.9.1.2 Features  i.MX 8M Plus Applications Processor Reference Manual

"HDMI TX includes the following features:
• Compatible with HDMI v2.0a spec
• Decode/encode the following video modes:
• All 2D video formats described in the CEA-861-F specification up to 4Kp30."

Supported resolutions can be found in driver "struct *cea_mode"

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/drm_edid.c?h=lf-5.10.y

https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/video/fbdev/mxc/mxc_edid.c?h=lf-5....

Since hdmi driver is the same as for i.MX6Q:   https://source.codeaurora.org/external/imx/linux-imx/tree/drivers/gpu/drm/imx/dw_hdmi-imx.c?h=lf-5.1...

one can try suggestions for i.MX6Q

https://community.nxp.com/t5/i-MX-Processors/iMX6Q-AI-board-support-for-1280-800-HDMI-Display/m-p/57...

 

Best regards
igor