error in component bean eeprom in 9s12g128

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

error in component bean eeprom in 9s12g128

2,471 Views
ThinkChip_Vendi
Contributor I

Hi, I have a error when I add the component eeprom, the error says 

+IEE1
+ERROR: Compiler option -CpPPAGE=0x15 (address of PPAGE register) or -CpPPAGE=RUNTIME must be set to compile the generated code correctly (current target settings, Compiler for HC12, Options, Code Generation tab, PPAGE register is used for paging). After compiler option change, run Code design to apply the change in Processor Expert. For details, see Help of the component.

+IEE1
+ERROR: There are errors in component, it is impossible to generate code

 

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

2,051 Views
ThinkChip_Vendi
Contributor I

I do all steps, and still have the same error, thanks

0 Kudos
Reply

2,051 Views
ProcessorExpert
Senior Contributor III

Hello,

 

could you please provide the verison of PE and CW that you use?

 

best regards
Vojtech Filip
Processor Expert Support Team

0 Kudos
Reply