Hi All
The appears to be no option to select a UART past UART 2 with PE as the debug console.
I'm using the FRDM-K22F dev board AND our own target board with same processor but higher pin count package and neither
processor allows you to select a UART higher than UART 2???
Also there is no option to select USB CDC as the debug console.
Is there a way to change this?
If not, will this be supported in a future release of PE?
Regards
Jerome
Hello Jerome Pitt:
The K22FN512xxx12 only has 3 UART (UART0/UART1/UART2) and 1 LPUART (LPUART0). That is why you cannot select UART3/4/5/...
As for the USB CDC option, that is not supported by Processor Expert. Try doing it manually as indicated in the next thread:
How do I setup the debug console to use the Virtual COM port (USB CDC driver)?
I hope this clarifies.
Regards!
Jorge Gonzalez