Will KDS support the KSDK filesystem with PE?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Will KDS support the KSDK filesystem with PE?

ソリューションへジャンプ
2,226件の閲覧回数
davepfaltzgraff
Senior Contributor I

I have been working on replicating the MQX USB Host demo but using the combination of KDS, KSDK, PE, and MQX. So far I'm making progress, but I find that I seem to be replicating the tasks that PE would do for me. For example, copying the source module msd_dsiskio.c and the corresponding include for include for msd_diskio.h.

Is there a plan for PE to ultimately include functions like the the file system? If so, when?

Maybe I should ask: Is it there now and I just don't know about it?

1 解決策
1,971件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello David,

Processor Expert does not support USB Host and filesystem SDK drivers now, i.e. there are not Processor Expert components that encapsulated these SDK drivers. I have created a new feature request for Processor Expert development team (PEXMCU-2178).

Best Regards,

Marek Neuzil

元の投稿で解決策を見る

4 返答(返信)
1,972件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello David,

Processor Expert does not support USB Host and filesystem SDK drivers now, i.e. there are not Processor Expert components that encapsulated these SDK drivers. I have created a new feature request for Processor Expert development team (PEXMCU-2178).

Best Regards,

Marek Neuzil

1,971件の閲覧回数
adyr
Contributor V

I have also spent a couple of days doing the same thing as David and eventually managed to get FatFs working on USB. Thank you Marek for adding a feature request for this.

Adrian.

0 件の賞賛
返信
1,971件の閲覧回数
davepfaltzgraff
Senior Contributor I

Hi Marek,

I suspected that this might be the case, but before I tag the question as answered, I am interested in learning more about the process. However, the link behind your reference to PEXMCU-2178 only lead me to a "server not found" message.

Can you investigate and/or provide additional pointers?

Thanks,

Dave

0 件の賞賛
返信
1,971件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hi David,

The ticket is available in a Freescale internal database and the ticket will go through approval process now.

You have not access to the database if you are not connected to Freescale intranet (e.g. you are a Freescale contractor or an employee).

Best Regards,

Marek Neuzil

0 件の賞賛
返信