Using IW610F as concurrent mode

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Using IW610F as concurrent mode

73 Views
TaeHyeok
Contributor I

Hi, NXP Team.

 

I have a question with using IW610F as concurrent mode. (at murata Type2KL module)

→ Using "AP (Wi-Fi)" mode & "STA (Wi-Fi)" mode & "BLE" simultaneously.

Is it possible to use all 3 functions simultaneously, without disconnection?

 

I think AP and STA mode should us 5G signal together and BLE will use 2G signal.

Is it possible to use in this condition?

→ If I see Murata's Type2KL datasheet, there's a filter that divide 5G and 2G.
    So, I assume that BLE will using 2G freq., so Wi-Fi can't use it.
    So, I think that AP and STA mode should use 5G freq. together.

→ In my recognition, AP should keep connect, so there would be a difficulty with using STA simultaneously. (The background of my thought)

Also, if there's something strange with my recognition, please notice me.

IW611 END-NODE-MATTER-WI-FI 

Best Regards.
Happy hump day.

 

0 Kudos
Reply
2 Replies

62 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

Please refer to the following release notes for the supported coexistence scenarios:

FreeRTOS
Linux

Regards,
Daniel

 

0 Kudos
Reply

57 Views
TaeHyeok
Contributor I

Hi. Daniel.

Really thank you for your reply.

 

I checked the Link you shared and there's some questions.

1. I think "Concurrent" and "Coexistence" function is a bit different.
   And, as it is written in NXP site, it seems IW610 series do support "Coexistence".
   And this do help customer to use different functions simultaneously. (Exactly it is not simultaneously)
   Do my recognition correct?

2. If I check the parts of Coexistence, there's no specific comment about using "AP + STA + BLE".
    Is it okay, that IW610 series do support coexistence of "AP + STA + BLE" ?
    Attached pic. do only say "BLE + Wi-Fi", so I think it do not clarify with my thought, so want to check.

TaeHyeok_0-1794453239507.png

Also, If I check at the another page you shared.
(mwifiex/doc/Release_Notes/Linux_RN/topics/coexistence.md at doc_WCT_release · nxp-imx/mwifiex · GitH...
It seems IW610 series do support "AP+BLE" or "STA+BLE".
But, there's no comment about "AP+STA+BLE", so I want to check, IW610 series do support this.

TaeHyeok_1-1794453513075.png

 

3. Also, Do all the FW (or SW) released by NXP do support this coexistence, as it is written in these pages?
    or, specific FW do support this coexistence?

Best Regards.
Have a nice day.

 

0 Kudos
Reply