SYSTEM_SMC_PMPROT_VALUE and high speed mode in K66

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SYSTEM_SMC_PMPROT_VALUE and high speed mode in K66

1,527件の閲覧回数
PeterFromSweden
Contributor III

When using K66 to set up 180 MHz high speed mode the SMC->PMPROT register must be set to allow high speed mode. In KSDK 1.2.0 system_MK66F18.h sets SYSTEM_SMC_PMPROT_VALUE to 0. Since this register is a one time writeable after reset it is not possible to change this.

Basic objective should be that Processor Expert clock configuration should be possible to use also for high speed mode.

/Peter

Realized that this is a processor expert question only...

タグ(1)
0 件の賞賛
返信
1 返信

1,354件の閲覧回数
vfilip
NXP Employee
NXP Employee

Hi,

you can set in in CPU component. Anyway we will improve this in next release of ProcessorExpert for Kinetis SDK.

pastedImage_1.png

best regards

Vojtech Filip

0 件の賞賛
返信