SBC uja1169 CMC configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SBC uja1169 CMC configuration

Jump to solution
3,319 Views
fk1
Contributor I

Hi,

I'm using the SBC UJA1169 middleware component

after being unable to perform CAN communications, i noticed that the processor expert output sets the CMC inside the CAN control register to SBC_UJA_CAN_CMC_OFMODE,
f i manually change the CMC in the config to SBC_UJA_CAN_CMC_ACMODE_DD, i can get the processor to receive CAN data.

how do i get processor expert to automatically set the CMC to another value, i can not see anything in the configuration what looks like it would change this?

 

note: I'm using S32 DS 2.0 on the processor S32K144

fk1_0-1626868870561.png

fk1_1-1626869161137.png

 

 

0 Kudos
Reply
1 Solution
3,305 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

checking the same in my S32DS2.2 with SDK RTM 3.0.3 I see option for mode selection

PetrS_0-1626942081487.png

So I can recommend to update S32DS and SDK; refer to https://community.nxp.com/t5/S32-Design-Studio/bd-p/s32ds

BR, Petr

View solution in original post

2 Replies
3,306 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

checking the same in my S32DS2.2 with SDK RTM 3.0.3 I see option for mode selection

PetrS_0-1626942081487.png

So I can recommend to update S32DS and SDK; refer to https://community.nxp.com/t5/S32-Design-Studio/bd-p/s32ds

BR, Petr

3,292 Views
fk1
Contributor I

Hi Petr,

 

I downloaded S32 DS 3.4, and that setting is also available

fk1_0-1627304953454.png

 

 

Thanks

Fahed

0 Kudos
Reply