Processor Expert Support for K26

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert Support for K26

1,698件の閲覧回数
thomasolenik
Contributor III

Are there any plans to support the K26 in KDS Processor Expert? The availability of PE support is a major factor in MCU selection for me. If I have a project that can be done with an MCU supported by PE, I use it. Not having PE support opens the decision up to other competitive product lines.

0 件の賞賛
返信
2 返答(返信)

1,451件の閲覧回数
BlackNight
NXP Employee
NXP Employee

Hi Thomas,

if you add the SDK V1.3 from Welcome to Kinetis Expert | Kinetis Expert , then you can create SDK V1.3 Processor Expert projects

pastedImage_1.png

But it is true that there is no Processor Expert any more with the SDK V2.0.

I hope this helps,

Erich

0 件の賞賛
返信

1,451件の閲覧回数
thomasolenik
Contributor III

Interesting. I don't think I've ever selected SDK and PE at the same time. A lot of my projects require CAN and the SDKs are a little weak for CAN bit timing. PE makes it so easy. 

0 件の賞賛
返信