Processor Expert Software - Microcontroller Driver Suite

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Processor Expert Software - Microcontroller Driver Suite

Processor Expert Software - Microcontroller Driver Suite

Product Information on Freescale.com

Product Summary Page

Documentation

Downloads

Training

Frequently Asked Questions (FAQ)

Where can I find Processor Expert examples and tutorials in Driver Suite?

How to configure the processor component to match my hardware?

Adding Processor Expert to C Project (without SDK in PEx Driver Suite)

Adding Processor Expert to C Project (with SDK in PEx Driver Suite)

Application Notes

AN4819 - Building a Project using IAR Eclipse Plugin - This application note provides steps to configure IAR Eclipse plugin and using Processor Expert (PEx) together with IAR build tool chain.

AN4913  - Building and Debugging a project using Keil MDK-ARM Eclipse plug-in - This application note provides steps to configure Keil MDK-ARM Eclipse plug-in and using Processor Expert together with Keil build tool chain.

Other Resources

Processor Expert Tools in Microcontroller Driver Suite - Training Videos

コメント

When will the following processor be added to the Processor Expert Suite?

Kinetis K65: 180MHz Cortex-M4F up to 2MB Flash (169pin) Applicable Parts:

Thank you.

The Microcontroller Driver Suite will not be extended with new parts lik the K65. You can use Kinetis Design Studio V3.x for this, see

https://mcuoneclipse.com/2015/06/28/tutorial-using-kinetis-design-studio-v3-0-0-with-iar-and-keil-id...

This offers (with the SDK V1.3) MK65 support:

pastedImage_2.png

With this, KDS v3.x (I recommend KDS V3.2, see https://mcuoneclipse.com/2016/04/02/nxp-kinetis-design-studio-v3-2-0/). Be aware that the future is with the Kinetis SDK and the SDK V2.0, see https://mcuoneclipse.com/2016/01/29/first-nxp-kinetis-sdk-release-sdk-v2-0-with-on-demand-package-bu....

I hope this helps,

Erich

Thank you Erich. I was able to access what I needed once I transferred to KDS V3.2 and installed SDK V1.3.

評価なし
バージョン履歴
最終更新日:
‎10-06-2012 01:34 PM
更新者: