Problem with Processor Expert command line generation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with Processor Expert command line generation

1,377 Views
abaa
Contributor I

Hello,

I'm trying to build PEx object from Jenkins(or from command line).

This are steps, which I want to do:

1) Import project into workspace - works

2) Generate PEx code - code is generated but kinets process never exits.

3) Synchronize PEx static code - how to do it?

4) Compile - this is simple

So I have question regarding step two.

This is how I'm calling PEx:

In my project directory:

First import project into workspace, works:

"c:\Freescale\KDS_v3\eclipse\eclipsec.exe" --launcher.suppressErrors -nosplash -application org.eclipse.cdt.managedbuilder.core.headlessbuild --launcher.ini "c:\Freescale\KDS_v3\eclipse\kinetis-design-studio.ini" -data "C:\Program Files (x86)\Jenkins\workspace\KDS" -import "."

Then generate PEx code:


"c:\Freescale\KDS_v3\eclipse\eclipsec.exe" --launcher.suppressErrors -nosplash --launcher.ini "c:\Freescale\KDS_v3\eclipse\kinetis-design-studio.ini" -data "C:\Program Files (x86)\Jenkins\workspace\KDS" -application com.freescale.processorexpert.core.PExApplication -generateAll

It generates PEx code(without synchronizing static code), but it hangs after that. Process never exits.

(There is no difference whether you call kinetis-design-studio.exe or eclipsec.exe with configuration file, so this is not the problem).

Here is the output:

Opening project LakeView-PS ...
generating

Here is log from workspace:

!SESSION 2017-02-15 22:47:32.708 -----------------------------------------------
eclipse.buildId=3.2.0.201603041649
java.version=1.7.0_76
java.vendor=Oracle Corporation
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_US
Framework arguments: -product com.somniumtech.branding.kds.ide -application org.eclipse.cdt.managedbuilder.core.headlessbuild -import .
Command-line arguments: -os win32 -ws win32 -arch x86 -product com.somniumtech.branding.kds.ide -application org.eclipse.cdt.managedbuilder.core.headlessbuild -data C:\Program Files (x86)\Jenkins\workspace\KDS -import .

!ENTRY org.eclipse.cdt.core 1 0 2017-02-15 22:47:48.288
!MESSAGE Indexed 'LakeView-PS' (20 sources, 25 headers) in 0.65 sec: 774 declarations; 2,604 references; 138 unresolved inclusions; 2 syntax errors; 470 unresolved names (12%)
!SESSION 2017-02-15 22:47:51.402 -----------------------------------------------
eclipse.buildId=3.2.0.201603041649
java.version=1.7.0_76
java.vendor=Oracle Corporation
BootLoader constants: OS=win32, ARCH=x86, WS=win32, NL=en_US
Framework arguments: -product com.somniumtech.branding.kds.ide -application com.freescale.processorexpert.core.PExApplication -generateAll
Command-line arguments: -os win32 -ws win32 -arch x86 -product com.somniumtech.branding.kds.ide -data C:\Program Files (x86)\Jenkins\workspace\KDS -application com.freescale.processorexpert.core.PExApplication -generateAll

!ENTRY org.eclipse.core.resources 2 10035 2017-02-15 22:47:52.251
!MESSAGE The workspace exited with unsaved changes in the previous session; refreshing workspace to recover changes.

My KDS version is 3.2.0, I have tried on second computer with fresh install, same happens.

Does anyone know the solution?

Lukas

0 Kudos
Reply
0 Replies