Nothing generated after clicked on "Generate Code"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Nothing generated after clicked on "Generate Code"

2,131 Views
jilingshu
Contributor I

hi all,

I tried to use "Device Initialization" to generate some basic code of my project. After set all modules required, I clicked on the "Generate Code" button, and window with provess bar shown. After the window disappered, no error reported, but there are also no MCUInit.c generated in Source or other folders.

 

BTW: I saw this error when starting CW10.1:

Starting local engineStarting SAE process.Internal CT_HOME=D:/Program Files (x86)/Freescale/CW MCU v10.1/analysis/1.1.0/Starting Engine with command: "D:/Program Files (x86)/Freescale/CW MCU v10.1/analysis/1.1.0/lib/host/vendor/win/python-2.5/python" -i "D:/Program Files (x86)/Freescale/CW MCU v10.1/analysis/1.1.0/lib/host/engine/codetest.pyc" --cli --inspect --namespace=I:/Test2/Freescale/workspace/.metadata/.SA/ct.ior.bearSAE process started."RootPOA" resolved and activated.Engine failed to create the IOR string file for the root factory. Aborting connection.

 I don't know what it means...

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,924 Views
ProcessorExpert
Senior Contributor III

Hello,

 

could you please try the same in CW V10.2?

 

Direct link to download:

http://cache.freescale.com/lgfiles/devsuites/HC08/CW_MCU_v10.2_SE.exe?fpsp=1&WT_TYPE=IDE%20-%20Debug...

 

best regards
Vojtech Filip
Processor Expert Support Team

0 Kudos
Reply