MPC 5775E LED blinking

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC 5775E LED blinking

2,331 Views
Krishna_Yalamanchili
Contributor I

Hi,

I have taken hello world example from MPC5777C to blink LED on MPC5775E.Unfortunately LED is not blinking. What am I doing wrong?

0 Kudos
Reply
2 Replies

2,070 Views
RachelGomez123
Contributor I

Another thing that commonly causes flickering in LED bulbs is loose connections or circuits. This is easy to fix. Just screw the LED bulb in tighter to see of that fixes the problem. If there's a lot of dust in the fixture, first blow out the connection points to remove the dust before putting the bulb back in.

 

Regards,

Rachel Gomez

0 Kudos
Reply

2,311 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

attached is working project for MPC5775E-EVB (S32DS 2.1 and SDK RTM 3.0.3). You just need to use wire to connect pin PTF[20] to LED. So, connect pin 2 of J125 header to some LED on JP6 header.

lukaszadrapa_0-1656070383095.png

Hope it helps.

Regards,

Lukas

0 Kudos
Reply