How to update LPC5526 firmware in mass production

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to update LPC5526 firmware in mass production

916件の閲覧回数
_Ferrari_
Contributor V

Dear all,

I develped a firmware for NXP5526 processor an now I want to update it during mass production.

I know that there is a ROM BOOTLOADER in NXP LPC552x/S2x MCUfamily so I want to use it to write firmware via USB0 in the internal empty flash.

So I have some questions

1) How to activate the ROM BOOT in the LPC552x processor family ?

2) What is the program on PC that I have to use ?

3) What is the correct procedure to update it ?

Thank you very much for your help and cooperation

best regards

0 件の賞賛
返信
1 返信

884件の閲覧回数
RaRo
NXP TechSupport
NXP TechSupport

Hello @_Ferrari_,

Unfortunately, there is not an application note or tutorial on how to do it through USB, so please look at the LPC552x/S2x User Manual. Chapter 6. Boot ROM and Chapter 7. Secure Boot ROM, it may be useful to look at.

Also, as a recommendation, please use USB1 instead of USB0, you can look the reason behind this in this post: [LPC55] Don’t Use ISP USB0 for firmware update - NXP Community.

Finally, you could take a look at the following links:

They might be useful. Hope this helps.

Best regards, Raul.

0 件の賞賛
返信