How can I get a package for the MK60DN512ZCAB (120 WCLSP) ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How can I get a package for the MK60DN512ZCAB (120 WCLSP) ?

1,198 Views
johnwoods
Contributor I

I don't see the 120 WCLSP package available. Is there a way to create a custom package or can I download one somewhere?

Tags (5)
0 Kudos
Reply
1 Reply

1,121 Views
BlackNight
NXP Employee
NXP Employee

Yes, that package is not listed. However, from a software perspective what counts are the pins which are routed to the package (independent which packages is used). So from this perspective, the BGA (ball grid array) package is what you could use instead?

0 Kudos
Reply