Generated Code and ISRs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Generated Code and ISRs

1,868 Views
ERussell
Contributor IV

I must have misunderstood the documentation but I was under the impression that any user changes to the PE generated ISRs would not be overwritten. However, my changes are being overwritten. For instance, I want to make changes to the PE_ISR(GPIO2_Interrupt) interrupt routine generated by PE. Is there something else I need to do so that these changes won't be overwritten?

 

Or better yet, define my own ISR function in another file outside of PE. Is there a way to communicate the name of my ISR function so that it gets added to the ROM vector table instead of the one generated by PE? My code copies the vector table to RAM so I could interject it then.

 

Thanks.

 

 

0 Kudos
Reply
1 Reply

1,667 Views
ProcessorExpert
Senior Contributor III

Hello,

 

could you please specify what version of PE, CW do you have? Could you please provide a step-by-step process that leads you to this behaviour?

 

 

best regards
Vojtech Filip
Processor Expert Support Team

0 Kudos
Reply