FRDM-KL02Z Board Support File

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FRDM-KL02Z Board Support File

1,486 Views
jayschwichtenbe
Contributor I

Don't want to waste my time reading the FRDM-KL02Z schematics and KL02 data sheets to figure out how to setup Processor Expert for the FRDM-KL02Z board.

Is there a Processor Expert board support file for the FRDM-KL02Z board?

If not is there any info/suggestions on how the hardware is configured to set it up for Processor Expert?

Thanks

Jay S.


0 Kudos
Reply
1 Reply

1,212 Views
BlackNight
NXP Employee
NXP Employee

Hi Jay,

I have created an example project with Processor Expert, available on GitHub.

It has FreeRTOS and LEDs, and does not include the other components of the board.

It uses additional Processor Expert components: see Processor Expert Component *.PEupd Files on GitHub | MCU on Eclipse how to download and install them.

But I should be able to easily add that if this is what you need.

0 Kudos
Reply