Does Processor Expert support setting up the FRDM-FXS-MULTI?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Processor Expert support setting up the FRDM-FXS-MULTI?

1,337 Views
defioren
Contributor I

Hi all,

I'm trying to get the SD card to work on the FRDM-FXS-MULTI which is mounted on the FRDM-KL25Z128 board. I was hoping to use Processor Expert to enable all the settings/interrupts easily to simply read and store the values from the various sensors on-board. Is there any example code for this? Is it supported with Processor Expert? Do I need any additional libraries downloaded for this support?

Any advice would be greatly appreciated!

0 Kudos
Reply
1 Reply

1,235 Views
marek_neuzil
NXP Employee
NXP Employee

Hello,

I am sorry, we have not any demo application or components for the FRDM-FXS-MULTI board now. You can find some components that support sensors on the page http://mcuoneclipse.com (e.g. magnetometer MAG3110). There is also a Git repository on the page https://github.com/ErichStyger/mcuoneclipse where you can download these components.

Best Regards,

Marek Neuzil

0 Kudos
Reply