Cpu_SetFlexNVMPartition() error on KDS3.2 +PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cpu_SetFlexNVMPartition() error on KDS3.2 +PE

1,894件の閲覧回数
Fan_xy
Contributor III

Hello ,

KDS 3.2 , TWR-K20D72M

Configure the FlexNVM partition on PE , then use the function Cpu_SetFlexNVMPartition() to set it ,

while when debug , i check the bit of "ACCERR" is set to 1 , and also it can not finish the partiton .

i have attached the project , please help me , thank you very much !

pastedImage_0.png

pastedImage_1.png

Thank you very much !

Fan

0 件の賞賛
返信
3 返答(返信)

1,490件の閲覧回数
marek_neuzil
NXP Employee
NXP Employee

Hello,

I have already provide answers and possible reasons of this issue. Please, see the discussion thread Return ERR_FAILED when calling Cpu_SetFlexNVMPartition() using KDS, PE and K10

You can also find a demo application for the SetFlexNVMPartition() method, see the discussion thread Reset when calling SetFlexNVMPartition() using KDS, PE and K22

Best Regards,

Marek Neuzil

0 件の賞賛
返信

1,489件の閲覧回数
Fan_xy
Contributor III

attachment

0 件の賞賛
返信

1,489件の閲覧回数
Fan_xy
Contributor III

Any help will be appreciate .

Thank you very much !

0 件の賞賛
返信