Consistency of project for several CPUs

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Consistency of project for several CPUs

1,940件の閲覧回数
ozillator
Contributor I

Hi, in our group we're using two different hardware generations, one is 56F803 based, the new one 56F8357. We got one top level bean that incooperates another bean, which vary with the CPUs, e.g. the CAN implementations (MSCAN, FLEXCAN). We approached the issue of adapting to the underlying CPU by including the hardware dependable beans in boolean groups which are then activated or disactivated. But somewho this approach is causing trouble when switching from one CPU to the other.

What is a good style to keep a project in such a case consistent. Obviously this has to be handled within the .chg file of the top level bean.

Thanks in advance for any kind of input! Steffen

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,718件の閲覧回数
ProcessorExpert
Senior Contributor III

Hi,

 

could you be please more specific how your component is designed  and what kind of trouble do you encounter ? The beast would be to have an example showing the problem...

The FreescaleCAN component should cover both MSCAN and FLEXCAN peripherals, even though it behaves differently - there may be some specific parts needed for each version.

 

 

best regards
Petr Hradsky
Processor Expert Support Team


0 件の賞賛
返信