CodeWarrior for MCU V6.3 Processor Expert V3.09 Update

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior for MCU V6.3 Processor Expert V3.09 Update

2,147 Views
grzegorzsobczyk
Contributor I

Hello,

I'm developing automotive projects on S12 and I'm trying to add FreeRTOS component to CWv5.1 or CW5.2.
I try to use components from this site : FreeRTOS  but I need to update my PE to v3.09.
Links to this update are obsolete: http://www.freescale.com/webapp/sps/download/license.jsp?colCode=CW08_V6_3_PE_V3_09_SP&nodeId=015210... 
I cannot find this update anywhere on NXP site. Does anyone know where I can find it?

Thanks for all the help!!

BR

Greg

0 Kudos
Reply
4 Replies

2,020 Views
grzegorzsobczyk
Contributor I

Hi Erich,
I've copied wrong link - actually I used your up-to-date components. I made it work on CWv5.2 and PE v3.06.
Still figuring out correct mcu/freertos configuration though. 
BTW thanks for all the good work on those mcu's and environments from medieval era! :smileywink:

BR

Greg

0 Kudos
Reply

2,020 Views
BlackNight
NXP Employee
NXP Employee

Hi Greg,

glad to hear that :-).

Just in case you have not seen that one: Back to Classic: FreeRTOS for Freescale S12(X) | MCU on Eclipse 

Erich

0 Kudos
Reply

2,020 Views
BlackNight
NXP Employee
NXP Employee

Hi Greg,

that FreeRTOS version is provided there for legacy reasons only. Nothing wrong if you are going to use that one, but the latest and greatest (maintained) version is available here:

McuOnEclipse - Browse /PEx Components at SourceForge.net 

Erich

0 Kudos
Reply

2,020 Views
grzegorzsobczyk
Contributor I

Found it here CodeWarrior® for Microcontrollers-Classic IDE|NXP   

Please close this topic

0 Kudos
Reply