CAN bus issue on FRDM-KE06Z: did anyone experience sending CAN frame issue?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN bus issue on FRDM-KE06Z: did anyone experience sending CAN frame issue?

1,709 次查看
peterbai
Contributor I

I created Processor Expert project using  CAN_LDD with interrupt enabled. I can see the CAN interface receives CAN frames, but output frames are never sent out. I checked the MSCAN registers, they appear correct.

Did anyone ever experience similar issue?

Thanks!

0 项奖励
回复
1 回复

1,166 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Peter,

this question was answer in SR1-2056200551.

please refer an example project showing simple frame sending and reception for the FRDM-KE06 board, please find it attached. pe team have tested it on the board without problems.

It's using loop mode of the CAN device, which you can also enable using the property in the CAN_LDD component.

=========================================

this answer is for you. if it helps, please click on "correct answer" button. thanks!

Best Regards,

Zhang Jun

0 项奖励
回复