Bootloader to application jump issue in S32k116

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader to application jump issue in S32k116

Jump to solution
9,166 Views
Ramsai
Contributor I

Hi,

I am working on a bootloader in which all the steps are done but while jumping from boot to app there is an issue.

I am using the below mentioned boot to application jump code.

void goto_application(void)
{
void (*entry)(void);
uint32_t pc, sp;

INT_SYS_DisableIRQGlobal();

S32_SCB->VTOR=(uint32_t)(0xa000);
sp = *((volatile uint32_t*)0xa000);
__asm("ldr r0, =0xa000");
pc = *((volatile uint32_t *)(0xa000 + 4));
entry = (void (*)(void))pc;
entry();
}

The application base address is 0xA000.

I added the breakpoint in the code to check the register values are getting properly updated or not. And when the breakpoint hit the entry() in the code the register values got updated as you can see in the below screenshot.

Ramsai_0-1651225658136.png

But after entry() , program counter is jumped to 0xA33A location instead of 0xA004(pc value is given in the above code). Below screenshot refers to this point. 

And also the application code is divided into 3 blocks.

1st block address starts from 0xA000 to 0xA2E5 

2nd block address starts from 0xA400 to 0xA40F and

3rd block address starts from 0xA480 to 0x1FFFF.

Ramsai_1-1651225859107.png

Program counter is locating to the address which doesn't come in all 3 blocks .

So, could someone help me in fixing the issue with proper solution.

If working code is provided for boot to application jump would be highly appreciated.

 

Controller: MCU-S32K116

IDE-S32 DESIGN STUDIOS

COMPILER-IAR

 

Regards,

Ramsai

0 Kudos
Reply
1 Solution
8,936 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Another idea - what does happen when you put a breakpoint at the entry point? Does it stop there? I'm wondering if you stepped over C level instruction or if you performed asm step. I believe it should work if asm step is used. If it works, you can load elf file of your application to have better understanding what happened.

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Debug-multiple-elf-files-in-S32-...

Regards,

Lukas

View solution in original post

0 Kudos
Reply
13 Replies
9,102 Views
Ramsai
Contributor I

Hi Lukas,

Thanks for your quick response.

Yes, when I tested with my previously mentioned bootloader to application code the r5 value is not getting updated. I tried in many ways but I couldn't able to make the r5 value matching with value present in 0xA004 address.

So, could you able to send the sample code of bootloader to application jump of s32k116 controller.

 

Regards,

Ramsai.

0 Kudos
Reply
9,079 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Ramsai,

this is working code from AN12218:

 

/* Start address for the application received by the bootloader
* application vector table should start at this address
* */
#define APP_START_ADDRESS 0x1000

 

/* Check if a valid application is loaded and jump to it */
JumpToUserApplication(*((uint32_t*)APP_START_ADDRESS), *((uint32_t*)(APP_START_ADDRESS + 4)));

 

/**
* Used to jump to the entry point of the user application
* The Vector table of the user application must be located at 0x1000
*
* */
void JumpToUserApplication( unsigned int userSP, unsigned int userStartup)
{
/* Check if Entry address is erased and return if erased */
if(userSP == 0xFFFFFFFF){
return;
}

/* Set up stack pointer */
__asm("msr msp, r0");
__asm("msr psp, r0");

/* Relocate vector table */
S32_SCB->VTOR = (uint32_t)APP_START_ADDRESS;

/* Jump to application PC (r1) */
__asm("mov pc, r1");
}

 

Regards,

Lukas

0 Kudos
Reply
9,067 Views
Ramsai
Contributor I

Hi Lukas,

I tried with the given working code shared by you. But even after implementing the same in my code its not jumping to application.

Please find below screenshots captured while debugging. These are for your reference.

 

Here in below screenshot APP_START_ADDRESS is 0xA000.

image.png

 

image (1).png

 

image (2).png

 

Kindly help me in identifying and solving this issue.

 

Regards,

Ramsai.

Tags (1)
0 Kudos
Reply
9,048 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

...and maybe one more thing - are all interrupts disabled before calling this function?

0 Kudos
Reply
9,044 Views
Ramsai
Contributor I

Hi Lukas,

All interrupts are disabled before calling of JumpToUserApplication() function.

Please find below screenshot.

 

All interrupts disabled.jpg

 

Regards,

Ramsai.

0 Kudos
Reply
9,050 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Ramsai,

I need to see a few previous steps. Could you take a screenshots:

- content of memory at 0xA000

- content of core registers r0 and r1 when the program jumps to JumpToUserApplication()

- content of core registers when it reaches __asm("mov pc, r1");

Thanks,

Lukas

0 Kudos
Reply
9,043 Views
Ramsai
Contributor I

Hi Lukas,

1. Please find below screenshot regarding content of memory at 0xA000.

A000 address.jpg

 

2. Below screenshot will show you the content of core registers r0 and r1 when the program jumps to JumpToUserApplication().

R0 and R1 values.jpg

 

3. Below screenshot shows you the values of all the registers when it reaches __asm("mov pc, r1");

Register values.jpg

 

For your info.

 

Regards,

Ramsai.

 

 

0 Kudos
Reply
9,038 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

It works as expected.
At 0xA000, there's value 0x20003800 which is supposed to be loaded to stack pointer.
At 0xA004, there's value 0x0000BC69, so your entry point of application is at 0xBC68 (+1 is used for thumb instruction set).
On the last screenshot, I can see that the msp and psp are set to 0x20003800 which is correct. And it's going to move r1 (0xBC69) to program counter which is also correct.
I can see nothing wrong here.

Could you check in map file of your application if 0xBC68 is really your entry point? And could you also check if there's expected code at this address?

Regards,
Lukas

0 Kudos
Reply
9,029 Views
Ramsai
Contributor I

Hi Lukas,

Thanks for the confirmation.

When the debugger reaches the __asm("mov pc, r1"); r1 is getting updated with 0xBC69 but when I click on step-in after this step the code is keep on running so I clicked on suspend option. 

When it is suspended it is showing that code is in 0xBA96 location and after this even though I keep on clicking on start button also it is showing as 0xBA96 location only.

Please find below screenshots regarding this.

Code is keep on running after __asm("mov pc, r1");

After r1 is BC69 .jpg

 

After suspending the code, pc is at 0xBA96.

PC reaching BA96 after giving BC69.jpg

 

I am also sharing you the values at these memory locations(0xBA96 and 0xBA69) and these are highlighted.

BA96 and BC68 register values.jpg

 

And also I am sharing you the screenshot of the map file at these locations.

Map file.jpg

 

 

Please look into this and do the needful.

 

Regards,

Ramsai.

 

0 Kudos
Reply
9,014 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Ok, it looks like there's valid opcode at entry point.

Could you send me a screenshot of these registers?

lukaszadrapa_0-1651850634195.jpeg

Thanks,

Lukas

0 Kudos
Reply
8,971 Views
Ramsai
Contributor I

Hi Lukas,

Please find below screenshot of the registers.

image (3).png

 

Regards,

Ramsai.

0 Kudos
Reply
8,937 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Another idea - what does happen when you put a breakpoint at the entry point? Does it stop there? I'm wondering if you stepped over C level instruction or if you performed asm step. I believe it should work if asm step is used. If it works, you can load elf file of your application to have better understanding what happened.

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Debug-multiple-elf-files-in-S32-...

Regards,

Lukas

0 Kudos
Reply
9,130 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Ramsai,

0xA004 is not entry point address and the code should not jump there.

There's reset vector at address 0xA004. And this reset vector then points to entry point of your application. Value in r5 register should be equal to value placed at 0xA004 and it should jump to this address. Could you check this? I can see in the screenshot that no application is programmed at this area.

Regards,

Lukas

0 Kudos
Reply