动力和电气化模拟驱动器知识库

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Powertrain and Electrification Analog Drivers Knowledge Base

讨论

排序依据:
Layout recommendation, critical component selection for PT2001. Document is also valid for PT2000, MC3316
查看全文
Hello All, I would like to share a bare board I designed to test one of our H-bridges. The design is based in the MC33926​ which is a DC motor driver, capable of handling up to 5A and 5 to 28v. The microcontroller I used to drive the H-bridge was the S08PA16 ​an 8-Bit, 5v microcontroller with Robust GPIO and high drive capability. Since I wanted to use this board for another projects, I leave access to 6 GPIO and 2 ADC-CH. The schematic and board design are compatible with CADSOFT EAGLE. I modified the Element14 library to add the uC and the H-bridge. I sent the gerber files to OSH Park, and hand solder everything to the board using solder paste. The uC was programmed with a Multilink BDM​. MC33926 Bare board Mounted devices The DC motor I was using did not require more than 3amps. However, the MC33926 is designed to handle up to 5amps and since I will use this board for any other project involving a DC motor, I designed a custom aluminum heatsink and manufacture it with a milling machine. The holes in the heatsink are centered with the VCC and DC-Motor connector screws, hence neither the connector screws or the header pins are in contact with the heatsink. I used thermal grease to properly mount the device on its heatsink. Final board: I hope this information helps anyone who would like to use our H-bridges. Please do not hesitate to contact me if you have any question. Regards, Josh
查看全文
​Vset: Set voltage. In LIN mode, The regulation voltage​ set by LIN RX frame. //设定调节电压。LIN调节模式下,Vset为LIN协议RX帧设定的调节电压值;默认模式下,Vset为OTP中写入的默认调节电压。 Vreg:Regulation voltage. the actual value that device regulate. During Thermal compensation or LIN timeout, Vreg is not equal to Vset. //调节电压。芯片实际工作中调节的目标电压值。温度补偿或者LIN超时,实际的调节电压Vreg会不等于Vset。  
查看全文
If you want to use MC33AR6000 to replace MC33TC80310 in a mature platform, should pay attention to some small difference on actions and diagnoses. See attachment for details.
查看全文
MC33AR6000 Driving code and Fusing code develop guide and example. Chinese version. MC33AR6000 驱动和烧录代码开发指导以及示例。中文版本。
查看全文
In pre excitation mode 2, you can have any duty cycle between pre exc value and 100% depending on battery and Vset voltage. On some alternators, with high duty cycles, the switching of excitation causes so much noise through the phase that this noise can be interpreted as valid phase signal. Thus, the device can go to regulation. To avoid that, we added the ability to deglitch the phase input only in pre excitation mode 2 to be sure that the signal we have are real phase signals. Depending on the duration of the noise our customer can see during pre excitation mode2, they can set the value of deglitcher. If they don't use pre excitation mode2, this value is "don't care".      
查看全文
1. Any of three kinds of fault trigger fault bit toggle to 1 OT: Temp>155℃ OC:short to battery/supply or over-current condition. OL:open load when OUTPUT OFF 2. base on truth table below, user can recognize the fault type   Output OFF(0) Output ON(1) HS Open load/ short to BAT(OC) short to GND(OC)/OT LS Open load/ short to GND(OC) short to BAT(OC)/OT   Open load(OL) and Short circuit base on Vds><Vout(FLT-TH) 33879   33880   OL: Vds<VFLT-TH && Output OFF Short to BAT: Vds > VFLT-TH && OC Short to GND: Vds< VFLT-TH &&OC  
查看全文
The attached GD3100 and GD3160 models may be used by customers in developing their schematic and PCB layout.
查看全文
This attachment helps you develop MC33879 replace MC33880.
查看全文