frdm-mcxa153

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

frdm-mcxa153

4,120 次查看
Asimoes
Contributor II

hello im a student and im willing to know if some of your boards are good or compatible with my thesis project.

So im looking to use an mcu to develop and ai to control and make correction on a traction inverter, for that i weas looking the frdm-mcxa153 and the inverter i was looking the FRDM-mc-lvpmsm and with the frdm-mc-lvmtb.

should i choose these boards or should i change to another ones. 

PD:they need to be development kits

标签 (2)
标记 (1)
0 项奖励
回复
5 回复数

4,102 次查看
Habib_MS
NXP Employee
NXP Employee

Hello @Asimoes,

The MCXA153 sounds good, but I could better recommend the MCXN947, since it includes an NPU that you could use for your AI. Additionally, there is already an application note that uses the FRDM-MC-LVPSMS on this page.

The SDK version where the example is found is mentioned on this same page, as shown in the next image:

Habib_MS_0-1747679273593.pngHabib_MS_0-1747679273593.png

 

Also, if you experience any issue, does not hesitate to let me know.

BR

Habib

0 项奖励
回复

4,083 次查看
Asimoes
Contributor II

So the idea would be to get the FRDM-MCXN947 and still with the frdm-mc-lvpmsm and the frdm-mc-lvmtb ?

or just like this picture, you think is possible to develop an ai based traction inverter?

Asimoes_0-1747772127102.pngAsimoes_0-1747772127102.png

 

 

0 项奖励
回复

4,059 次查看
Habib_MS
NXP Employee
NXP Employee

Hello again @Asimoes,

So, the idea would be to get the FRDM-MCXN947 and still with the frdm-mc-lvpmsm and the frdm-mc-lvmtb ?

Yes, the MCXN947 includes an NPU, which can enhance the performance of your AI applications.
Additionally, the FRDM-MC-LVPMMSM board is compatible with the MCXN947 and provides a 3-phase bridge inverter for motor control applications.

However, you will need to create and set up the AI models yourself, based on what your project needs.

Also, if you experience any issue, do not hesitate to let me know.
BR
Habib

0 项奖励
回复

3,686 次查看
Asimoes
Contributor II

Hello @Habib_MS,

 

im currently trying to use the setuup you recommended me but im getting some troubles to get the app to work . When im doing the debug on MCUxpresso IDE i receive this message, should this be a problem?

Asimoes_0-1751553404966.pngAsimoes_0-1751553404966.png

then when im trying to set the on on the application switch it doesnt let me do it, stays on off

Asimoes_1-1751553558664.pngAsimoes_1-1751553558664.png

on the video appears like this 

Asimoes_3-1751554594722.pngAsimoes_3-1751554594722.png

do you have any idea how to solve this problem?

 

Thanks in advance

 

 

0 项奖励
回复

3,677 次查看
Habib_MS
NXP Employee
NXP Employee

Hello @Asimoes,
Could you post your question in another community post?
Since it is a separate question from the original one, and to keep this thread separate. 
You can tag me in the other post to provide you support.
BR
Habib

0 项奖励
回复