Hello again @Asimoes,
So, the idea would be to get the FRDM-MCXN947 and still with the frdm-mc-lvpmsm and the frdm-mc-lvmtb ?
Yes, the MCXN947 includes an NPU, which can enhance the performance of your AI applications.
Additionally, the FRDM-MC-LVPMMSM board is compatible with the MCXN947 and provides a 3-phase bridge inverter for motor control applications.
However, you will need to create and set up the AI models yourself, based on what your project needs.
Also, if you experience any issue, do not hesitate to let me know.
BR
Habib