MC33HB2001 - Internal Pullups

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MC33HB2001 - Internal Pullups

ソリューションへジャンプ
4,893件の閲覧回数
deckhardt
Contributor IV

The datasheet indicates that the MC33HB2001 has internal pullups to 5V and I am questioning if this is correct when VDDQ of 3.3V is applied: 

deckhardt_0-1679926371006.png



When looking at the development board FRDM-HB2001FEVM it looks like you can connect VRDM_VDD to VDD and VDD to VDDQ.

Could someone confirm if these internal pullups are to VDDQ or is there an internal 5V regulator?

ラベル(1)
タグ(4)
0 件の賞賛
返信
1 解決策
4,880件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi David,

The pull-up level is dependent upon the voltage level applied to VDDQ. If 3.3V is applied on VDDQ, the internal pull-ups will be to 3.3V for these logic pins. I think the spec is referring to a 5.0V applied to VDDQ scenario.

Best regards,

Tomas

元の投稿で解決策を見る

3 返答(返信)
4,770件の閲覧回数
deckhardt
Contributor IV

I have laid out a development board using the MC33HB2001FKR2. I supplied 12V to VPWR (pins 12,13,29,30) and 3.3V to VDDQ (pin 1) and CS_B (pin 32) measures to be 0V. According to the datasheet the CS_B pin should be internally pulled up. Can you confirm or deny? I confirm the same behavior on the NXP development board FRDM-HB2001FEVM. 

0 件の賞賛
返信
4,756件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi David,

Yes, CS_B has an internal weak pull-up to VDDQ. The FRDM-HB2001FEVM development board drives the SPI signals at 3.3V. The MCU should not be holding the CS_B pin low while data is not being transmitted.

Best regards,

Tomas

0 件の賞賛
返信
4,881件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi David,

The pull-up level is dependent upon the voltage level applied to VDDQ. If 3.3V is applied on VDDQ, the internal pull-ups will be to 3.3V for these logic pins. I think the spec is referring to a 5.0V applied to VDDQ scenario.

Best regards,

Tomas