BATTERY MANAGEMENT SYSTEM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BATTERY MANAGEMENT SYSTEM

2,012 Views
rj2025
Contributor I

i am working on making a bms for fsae electrical vehicle  

i require 13 gpio pins in the cell monitoring unit for temperature monitoring  but in MC33774 only 8 GPIOs pins are present so is there a way to increase number of  GPIO pins by using some ic or by using two MC33774 ics together also if i use a centralized thermistor expansion module would it be able to communicate with s32k3 or will there be any problem 

thank you 

Labels (1)
0 Kudos
Reply
1 Reply

1,975 Views
ErikaC
NXP TechSupport
NXP TechSupport

Hello,

Yes, you can use multiple MC33774 ICs in the same BMS chain or you can check our GPIO Expanders: https://www.nxp.com/products/interfaces/ic-spi-i3c-interface-devices/general-purpose-i-o-gpio:MC_418...

0 Kudos
Reply