sdram data swapping

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

sdram data swapping

2,413件の閲覧回数
Pamid
Contributor II

I would like to know MPC885  databus(31:0) connectivity   to SDRAM  MT48LC2M32. Shall we need to connect D0 of MPC885 to D0 of SDRAM or D0 of mpc885 to d31 of SDRAM. As mpc885 is in big-endian  mode and connecting MPC885 A29--> SDRAM A0. as far as data bus is concerned  we need clarification.

ラベル(1)
  • DDR

0 件の賞賛
返信
1 返信

2,361件の閲覧回数
r8070z
NXP Employee
NXP Employee

You can swap byte lanes and bits inside byte lane as you want. For example you can connect byte lane D0, D1, D2..D7, BS0 of the MPC885 to D15, D13, D14…D8, DQM1 of the SDRAM MT48LC2M32. The MPC885 reads the same byte what it writes.

0 件の賞賛
返信