i.MX6 without an external POR circuit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6 without an external POR circuit

1,251 Views
fletcher_wang
Contributor I
How to configure the i.MX6 to operate without an external POR circuit?
0 Kudos
Reply
3 Replies

1,223 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

If the external POR_B signal is not used (always held high or left unconnected), the processor defaults to the internal POR function (PMU controls generation of the POR based on the power supplies). There is no need to configure it.

i.MX6ULL has a module that generates an internal POR_B signal that is logically AND'ed with any externally applied SRC_POR_B signal. The internal POR_B signal will be held low until all of the following conditions are met:

• 4ms after the external power supply VDDHIGH_IN is valid
• 1ms after the VDD_SOC_CAP supply is valid:

Best regards.

1,243 Views
JorgeCas
NXP TechSupport
NXP TechSupport

Hello,

Which i.MX6 are you referring for? Could you please share exact part number?

Best regards.

0 Kudos
Reply

1,228 Views
fletcher_wang
Contributor I

i.MX6ULL, MX6Y2CVM08AB

0 Kudos
Reply