Have a great day,
What should I do when I try to set 60x-Bus from Single-MPC8280 Bus Mode to 60x-Bus Compatible Mode? I already tried to set the BIT[0] of Bus configuration register(BCR[EBM]=1) in Vxworks (Uboot already run,and Single-MPC8280 Bus Mode default),but the system stuck and reset after because of hardware watchdog. There is 64-bit SDRAM,16-bit FLASH,16-bit DPRAM and 8-bit BootROM connected to the 60-Bus .
So what should I do when I try to set 60x-Bus from Single-MPC8280 Bus Mode to 60x-Bus Compatible Mode? It must be configured in Uboot?
Need to involve hardware changes? I see a message in the manual:if the MPC8280 is in 60x-Bus cpmpatible mode,BADDR[27-31] should be used instead of A[27-31]. BADDR[27-28] is floated and BADDR[29-31] is pulled up in my design.