choose powerPC main frequency

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

choose powerPC main frequency

1,513 次查看
jeffcao
Contributor I

I want to Know the relationship between the main frequency of MCU and the transmission bandwidth.

I don't know how to choose the main frequency of the chip.I need to achieve a balance between the main frequency and the power consumption.

标签 (1)
0 项奖励
回复
1 回复

1,354 次查看
r8070z
NXP Employee
NXP Employee


Have a great day,

I do not see what particular PowerPC chip and transmission type you mean. Typically if there is such  restriction then device reference manual describes that. For example the MPC8548e manuals says: For proper PCI Express operation, the CCB clock frequency must be greater than (500MHz)*(PCI Express link width) /8

TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复