Heinz Wrobel,
Thanks for the reply.
I have checked the PLL Clock and also PLL power supply filtering (getting required 1.2V). now I am using SDRAM for RAM requirement.But I still having issues with downloading the code as mentioned in query 2 and 3 repeated below.
ERROR 1. CANNOT PUT THE TARGET TO STOP MODE
On starting debugging the object code gets dumped into the configured RAM memory but we do not get control at the breakpoint. If we try to “STOP” program execution the following message pops up.
The same error message also pops up before code dumping into the RAM occasionally.
Attached are the Configuration file, debug.map, file and the CCS Log.
ERROR 2. RCWHR AND RCWLR values not loading from JTAG File.
On configuring the CodeWarrior USB Tap from the Remote Debugging Connection Settings window in Debug Version Settings of the CodeWarrior IDE 8.8 we find that the value given in the Reset Module registers is that as given in the FLASH rather than the value given in the JTAG configuration file. also find the attached log files and screen shots.