T1042 RCW source pins

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

T1042 RCW source pins

985件の閲覧回数
ankurkumar
Contributor I

Hello,

           We have multiple boards with a T1042 processor. So this problem is in only one card. Card specific problem.

 

       We are able to detect T1042 via Lauterbach cable and program SPI flash attached to it but the card doesn't boot. We have observed that we are getting strange values on RCW source pins which are only set by pull up/down resistors. and thus value of RCW source pins are not which we have set. it seems the processor is driving these pins. We are not able to understand why this happening. No other boards is behaving like this so it is essentially a hardware problem but not able to debug. Could you pl help us with what could be causing processor to behave like this.

0 件の賞賛
返信
1 返信

959件の閲覧回数
ufedor
NXP Employee
NXP Employee

Please provide additional information:

1) the processor connection schematics as searchable PDF

2) digital scope traces for the processor power supplies ramps

3) digital scope traces for the processor reset signals (as shown in the QorIQ T1040 Reference Manual, Figure 4-1. Power-on reset sequence) and RCW source signals behaviour during POR

0 件の賞賛
返信