Supported devices in the Code warrior 9.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Supported devices in the Code warrior 9.2

1,439 Views
maheshwarreddy
Contributor I

We are using the code warrior 9.2 and we have the target MPC5125 tower kit . While creating the project we are finding the target but its showing the only MPC5121 device only .

Thank you 

Best regards

Maheshwar.

0 Kudos
Reply
2 Replies

1,316 Views
Pavel
NXP Employee
NXP Employee

 

Install SP1 patch for the MPC5125. Load this patch using the following link to Google drive:

https://drive.google.com/open?id=1vQAgW6Dj7aNxCVYszgi2hObyClR67yzS


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply

1,316 Views
maheshwarreddy
Contributor I

Hai, Pavel Chubakov,

     Thank you for the reply.When we are going to debug mode it is showing that check your JTAG clock speed error .what may be the problem .

Best regards 

Maheshwar

0 Kudos
Reply