SUPPORTED IDE AND JTAG FOR MPC 866 PROCESSOR

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SUPPORTED IDE AND JTAG FOR MPC 866 PROCESSOR

4,982 次查看
skchethan123
Contributor I

I have installed Code warrior development studio for power architecture. But i didnt find a option to select MPC866 family in that tool.

i have installed 10.5 version.

标签 (3)
标记 (1)
0 项奖励
回复
8 回复数

4,711 次查看
Pavel
NXP Employee
NXP Employee

CodeWarrior 10.5 does not support the MPC866. Use CodeWarrior 8.8 for software developing and debugging for the MPC866:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

See also attached snapshots.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

4,711 次查看
jinyu_zhang
Contributor II

Does the 8.8 version be able to install in Ubuntu OS?

0 项奖励
回复

4,711 次查看
skchethan123
Contributor I

thank you for reply,

One more suggestion i want regarding suitable JTAG and drivers for SPI, UART and parallel bus for MPC866.

0 项奖励
回复

4,711 次查看
skchethan123
Contributor I

And even can i find drivers for SPI, UART and parallel bus anywhere.

0 项奖励
回复

4,711 次查看
skchethan123
Contributor I

Thank you for the reply sir,

i more suggestion i want, can i know that which is the suitable JTAG for MPC866

0 项奖励
回复

4,711 次查看
jinyu_zhang
Contributor II

search for Code Warrior USBTAP probe

0 项奖励
回复

4,711 次查看
skchethan123
Contributor I

Thank you for the information Mr. Zhang.

It will be helpful for me if you give any suggestion regarding peripheral drivers for MPC866

0 项奖励
回复

4,711 次查看
jinyu_zhang
Contributor II

Sorry for replying later. I have no idea about the probe's driver, however, it seems like that the driver is installed automatically. The information about the Code Warrior USBTAP probe, refer to the link:

USB TAP for PowerQUICC® I|NXP 

BR,

jinyu

0 项奖励
回复