SSL for MPC8309TWR LTIB can't installed

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

SSL for MPC8309TWR LTIB can't installed

1,107件の閲覧回数
ispark
Contributor I

Hello,

I configured the kernel for use ssh with ssl at ltib.

then while building target kernel, below error issued.

Processing: openssl

=====================

Build path taken because: no prebuilt rpm,

Try openssl-0.9.8g.tar.gz.md5 from the GPP

Try openssl-0.9.8g.tar.gz from the GPP

Can't get: openssl-0.9.8g.tar.gz at ./ltib line 790.

would you please let me know what is problem?

Thanks

IS

0 件の賞賛
返信
2 返答(返信)

977件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello IS Park,

openssl-0.9.8g.tar.gz and openssl-0.9.8g.tar.gz.md5 should be put in /opt/freescale/pkgs/ folder.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

977件の閲覧回数
ispark
Contributor I

it was network problem..

Thanks.

0 件の賞賛
返信